Loading...

Why Does my Timer Switch Not Automatically Adjust For Daylight Savings Time?

The VPT24-1PZ model has two programming modes: STD (Standard) and PRO. There is a setting that can be enabled in the PRO programming mode that will automatically adjust for Daylight Saving Time (DST). If the device was set up in STD (Standard) Mode or DST setting was not enabled you will need to manually adjust the time on the clock twice a year or enable the Daylight Saving Time feature.

If you live in an area that adjusts the time for Daylight Savings Time it is recommended to reprogram your VPT24 using the Pro Mode.  This video will show you how:

To Set the Time:

  • Place your fingers on the bottom of the switch paddle and gently lift it upward to open it until it clicks.
  • Press the MENU button until you see CLK appear and press the SET button.
  • Adjust the time using the UP or DOWN arrows and press the SET button after each setting.
PRO Programming for the Decora VPT24 24-Hour Programmable Timer Switch | Leviton

Pro Programming for the VPT24-1PZ 24-Hour Programmable Timer Switch

Related Products

Additional Support Material