Loading...

How do I know if my Decora Smart® device is HomeKit compatible?

Decora Smart has two series of products that are compatible with Homekit technology.  Decora Smart 1st Gen with Homekit technology products part numbers started with 'DH'.  In March 2021 the Decora Smart Wi-Fi 2nd Gen product officially started shipping that combines Decora Smart Wi-Fi with the Homekit technology and the part numbers begin with 'D2'.  

Decora Smart 1st Gen with Homekit Technology products (DISCONTINUED):

DH1KD - 1,000w Dimmer
DH6HD - 600w Dimmer
DH15S - 15A Switch

Decora Smart Wi-Fi 2nd Gen products:

D26HD - 600w Dimmer
D215S - 15A Switch
D215P - 15A Plug-in Switch
D23LP - 300w Plug-in Dimmer

Finding the Part Number:

Wall Box Devices:

  • Remove the wall plate
  • The device does not need to be removed from the wall
  • If you do remove the device from the wall, please be certain to turn off the power at the circuit breaker
  • On the front strap the part number is engraved or a sticker in the upper right corner
  • Reinstall the wall plate

Plug-in devices:

  • Unplug the plug-in switch or dimmer
  • On the side of the device with the prongs the part number will be listed on the sticker or embossed in the plastic