Loading...

Leviton launches new line of surge panels for multi-tiered protection and compliance with the latest NEC® requirements

Featuring improved performance and environmental ratings suitable for residential, commercial, and industrial applications

Melville, N.Y., October 10th, 2023 – Leviton today announced a new line of Type 1 and Type 2 surge protective panels in the most common voltage configurations, providing solutions for various applications from residential to commercial and industrial. With improved surge protection and environmental ratings, these new panels deliver industry-leading performance.

“Our priority is to provide customers with advanced solutions and the knowledge needed to effectively safeguard their systems,” said Tony Pulsonetti, director of product management, Leviton Commercial & Industrial. “Surge devices vary by type depending on the area they protect and where they are installed. Understanding how these layers work together is key for complete surge protection.”

By using the new panels alongside Leviton’s existing surge protected breakers, receptacles, and power strips, customers can have Type 1, 2, and 3 protection for valuable assets and critical equipment from the service panel outside the home or building to the point of use.

A major benefit of the new surge panels is that they are compliant with Article 230.67 of the National Electrical Code® (NEC). This article, introduced in the 2020 NEC, added a requirement for all services supplying dwelling units to be provided with a surge protective device (SPD), as an integral part of equipment or located immediately adjacent. The SPD must be Type 1 or Type 2. The 2023 NEC expanded upon Article 230.67 expanding “dwelling units” requiring an SPD to include dormitory units, guest rooms and suites of hotels and motels, as well as areas of nursing homes and limited-care facilities used exclusively as patient sleeping rooms.

The launch includes the R, P, B, M, and X Series, featuring NEMA 4 or 4X outdoor ratings and offering a range of solutions from compact and easily installed panels tailored for residential use, to cutting-edge panels featuring LCD screens and advanced functionalities such as surge counting and performance monitoring for industrial use.

For more information regarding Leviton’s complete surge offering and multi-tiered applications, visit Leviton.com/surge. 

About Leviton Commercial and Industrial

Leviton’s comprehensive line of commercial and industrial-grade electrical wiring devices provide builders, contractors and specifiers with solutions engineered to withstand the most rigorous commercial environments and harshest industrial applications. Leviton manufactures everything from commercial, industrial and hospital grade wiring devices, to surge protective devices, electric vehicle supply equipment, temporary power solutions, heavy duty motor starter switches, IEC and NEMA watertight rated devices and more. Learn more at www.leviton.com/commercial.

About Leviton

Every day, Leviton builds what’s next to light, power, and connect everyday spaces to meet the needs of its residential, commercial, and industrial customers globally. From controls, to lighting, to electrical, to networking, Leviton’s relentless innovation for more than a century enables our customers' lives to be easier, safer, more efficient, productive and sustainable. Driven by its commitment to its customers, the ingenuity of its employees, and the safety and quality of its products and solutions, with Leviton, the FUTURE IS ON. For more information, visit http://www.leviton.com/, www.facebook.com/leviton, www.twitter.com/leviton, or www.voutube.com/Levitonmfa.