Leviton GFCI's
All of our GFCI outlets and circuit breakers are engineered to help protect people from the hazards of electric shock and electrocution by interrupting power if a ground-fault is detected.
Where you need GFCI protection
GFCI outlets monitor the electrical power that is fed to anything plugged into the outlet. If a ground-fault is detected, it shuts off power to the item in a fraction of a second to help prevent serious injury or death. Ground faults occur when a current flows along an unintended path, such as through water or a person. For example:
- Operating electrical equipment in wet or damp conditions
- Electrical current leaks from appliances or tools
- Electrical wiring becomes frayed or damaged
GFCI protection is required in:
- Bathrooms
- Garages and Accessory Buildings
- Outdoors/Pools and Spas
- Basements
- Kitchens
Leading the Way in Slim GFCI Technology
A slim profile leaves more room in the wallbox for faster and easier installations.
Why choose a Leviton GFCI?
Protection without exception. Other manufacturers may allow their GFCI devices to be reset even after protection is permanently lost – taking advantage of UL exemptions and providing users with unprotected power. Why take chances? Additionally, our GFCIs sit closer to the wallplate for a polished appearance. Leviton SmartlockPro® outlets feature the slimmest profile on the market for easy installation, every time.
How Can We Help?
Do you have questions about our GFCIs?