Loading...

CIO Playbook

Download today

Download the playbook today

Building the Future of AI Data Center Networks

Cabling isn’t just “plumbing” anymore – it’s a strategic lever for performance, risk reduction, and ROI. This playbook explains why and how CIOs can successfully guide decision making for AI data center architectures.

16 pages | File Type: Adobe PDF | Size: 2.9 MB

 

EXCERPT: 

AI data centers look and feel very different from traditional facilities. The most striking difference is the sheer number of connections. In a conventional setup, traffic is aggregated through a limited number of ports, and bandwidth is shared. AI clusters, by contrast, favor non-blocking topologies where every server and switch is tied directly to every other device. Each additional layer multiplies the number of optical links, creating an exponential rise in fiber counts. For anyone stepping into an AI environment for the first time, the sight isn’t dominated by racks of servers, but by an overwhelming web of cables.

Power demands also escalate dramatically. Where a traditional rack might have drawn a handful of kilowatts, AI racks can easily surpass 100 kW. That kind of density raises serious challenges around cooling. Even small details like cable diameter and routing affect airflow, making physical infrastructure a critical part of thermal management.