- Away? Create a “lived-in” look for your home when you schedule lights to turn on and off at set or random times
- Never come home to a dark house again. Schedule porch and indoor lights to turn on before you arrive home
With no set-up, hub or internet required, programming and managing your lighting is made simple with Bluetooth* technology. Just download the free Decora Digital Dimmer & Timer App, pair with your smartphone or tablet, and get started.
![Modern exterior lighting on house](/adobe/dynamicmedia/deliver/dm-aid--6b9828bc-3b48-467e-bdf9-0d93fe6dc5cb/640x360-aem-outdoor-lights.jpg?preferwebp=true&quality=85)
Safety & Security
Convenience
- Movie night, entertaining and reading is more relaxing when you dim or raise the lights from the comfort of your couch, dining room table or bed
- Let your child drift off to sleep with the countdown/sleep timer. Simply program how long you want the lights to stay on and they'll automatically switch off for comfort and peace of mind
![Child in bed asleep](/adobe/dynamicmedia/deliver/dm-aid--dd745030-8fbe-4090-9682-37c935c3f725/640x360-aem-child-in-bed.jpg?preferwebp=true&quality=85)
Featured Videos
Decora Digital with Bluetooth Technology Products
Decora Digital Controls with Bluetooth Frequently Asked Questions
Click here for the answer.
Yes. All Decora Digital devices require a ground wire for installation.
If you remove the wall plate, there is a product label in the upper right hand corner of the metal strap.
Decora Digital requires that smartphones and tablets support Bluetooth 4.0 (BT LE), also known as Bluetooth Low Energy. The following iPhones® and iPads® use Bluetooth 4.0:
iPhone® | iPad® |
|
|
Apple: iOS 6.0 or later
Android: Android 5.0 or later
Android 7.1 or later (Android 7.0 is not supported)
No, the battery is permanently installed.
The DDS15, DDE06, DD710 and DDF01 all include a built-in backup battery that is used to keep track of the current time of day even in the event of a power loss. These devices have been designed to maintain the time for more than 72 hours without power.
The DDMX1 and DDL06-BL do not have this built-in backup battery, so you may need to reconnect your device to the Decora Digital Dimmer & Timer App to update to the current time in the event of a long or short-term power interruption.
Settings such as programmed events, minimum dim level, etc. are permanently programmed into the device. Power loss will not affect these settings and they will remain unchanged. For devices without a backup battery, such as DDMX1 and DDL06-BL, a connection will be required to update the time.
All Decora Digital controls (except for the DD0SR-1 Remote) have a locator light. The locator light is the small green LED light located below the rocker switch that illuminates when the load is off. This light is helpful in locating the device in the dark. This light can be disabled using the Decora Digital Dimmer & Timer app for users who choose not to have this light illuminated (DDL06-1L users must disable this manually).
DDMX1 | Dimmable LEDs, dimmable CFLs, incandescent, halogen, Mark10® Powerline, MLV |
DDL06 | Dimmable LEDs, dimmable CFLs, incandescent, halogen |
DDS15 | LED, CFL, incandescent, fluorescent, resistive, motor |
DDE06 | ELV, dimmable LEDs, dimmable CFLs, incandescent, halogen |
DD710 | 0-10V LED/Fluorescent Ballasts |
Resources
How Can We Help?
Visit our Decora Digital Knowledge Base for tips, videos and FAQs