Loading...

Power Outage Application Note

In the event of a power outage, the VPT24 Decora® 24-Hour Programmable Timer is equipped with a battery* backup so that the date and time settings will remain as indicated below:

  • The date and time will be maintained for up to 3 days (72 hours)
  • The programmable options and schedules are stored until factory reset.

*  Battery life may vary depending on a variety of variables including the age of the device and how often it is woken up during  an outage. As with cell phones and other electronics, the battery capacity in the VPT24 timer may decrease over time. 

For more information please visit the VPT24-1PZ or VPT24-16Z product page which includes product info, specifications, and marketing materials.

Related Video

PRO Programming for the VPT24-1PZ 24-Hour Programmable Timer Switch