Loading...

Setting the Minimum and Maximum Dim Levels of a Decora Smart® Zigbee Dimmer

Leviton Decora Smart Zigbee devices have the ability to alter the minimum dim level to increase compatibility with LED bulbs as well as alter the maximum brightness to save energy.


To change minimum dim level:

  • Enter Programming Mode by holding the top of the paddle for 7 seconds (the Status Light will turn amber), and then release (the Status Light will begin to blink amber).
  • Tap the top of the paddle 5 times. The Status Light will quickly flash red and amber.
  • Tap the top of the paddle 1 time. The Status Light will flash amber.
  • Use the dim/bright bar to adjust the minimum dim level.
  • Hold the top of the paddle to exit.

 To change maximum dim level:

  • Enter Programming Mode by holding the top of the paddle for 7 seconds (the Status Light will turn amber), and then release (the Status Light will begin to blink amber).
  • Tap the top of the paddle 5 times. The Status Light will quickly flash red and amber.
  • Tap the top of the paddle 2 times. The Status Light will flash red.
  • Use the dim/bright bar to adjust the maximum dim level.
  • Hold the top of the paddle to exit.