Loading...

Setting the Preset Light Level of a Decora Smart® Z-Wave Dimmer

Leviton Decora Smart Z-Wave Dimmers have the ability to alter the preset light level.

  • Enter Programming Mode by holding the top of the paddle for 7 seconds (the Locator LED will turn amber), and then release (the Locator LED will begin to blink amber).
  • Tap the top of the paddle 7 times. The Locator LED will quickly flash red and amber.
  • Use the dim/bright bar to adjust the desired preset light level.
    • Note: 0% or OFF disables the preset light level and will instead use the last level
  • Hold the top of the paddle to exit.
    • The Locator LED will quickly flash amber to confirm.