Loading...

Can I Mix Bulb Types With the Decora Digital™ Dimmer?

The Decora Dimmer is designed and tested with the expectation that all of the lighting loads are the same type. It is recommended that the same light source be used to achieve consistent performance. If you choose to mix bulb types on the same dimmer it is possible that you will experience a variation in dimming performance, start-up characteristics, and possible side effects such as flickering or noise.

Additionally, you can check out our LED Bulb Compatibility Tool.