Loading...

Where is the Decora Smart Wi-Fi Serial Number Located?

When working with Technical Services, you may be asked to provide the serial number for a Decora Smart® Wi-Fi device.  There are two easy ways to find the serial number, a screen in the My Leviton app or a sticker on the device.

Finding a Serial Number in the My Leviton App:

Click on the 3 dots [] in the upper-right corner of the device card and choose Settings.

Decor
Decora Smart

Choose Device Health and the serial number is shown in the Device Health screen.

Decora Smart
Decora Smart

Finding the Serial Number on a Decora Smart Wi-Fi Device

The serial number is on the front strap of the Decora Smart Wi-Fi switch or dimmer:

  • Remove the wall plate
  • The serial number will start with 100 and will be in xxxx_xxxx_xxxx format
  • There will only be numbers in the serial number
  • The location of the serial number will be a sticker placed on the top or bottom strap
Decora Switch
Decora Switch

The serial number is on the blade side of the plugin switch and dimmer:

  • Unplug the module
  • The serial number will start with 100 and will be in xxxx_xxxx_xxxx format
  • There will only be numbers in the serial number
  • The location of the serial number will be a sticker placed on the right or vertically on the side
Decora Serial Number
Serial Number