The Voice Dimmer can control dimmable LED, dimmable CFL, and Incandescent bulbs.
The Decora Smart™ Voice Dimmer with Amazon Alexa Built-in combines easy Wi-Fi lighting with the convenience of the Amazon Alexa voice assistant in a single, sleek device built into your home.
The Voice Dimmer allows users to fully automate their lighting with voice control, schedules, or remote access while also enjoying the many benefits of Alexa including music streaming, news updates, announcements and more – no additional Alexa device or hub needed.
Users can create an Alexa routine that gradually brightens their lights in the morning when they are waking up while also giving them the news of the day and a traffic update before they head out to work.
The Voice Dimmer connects to Wi-Fi and uses the My Leviton app. Pairing the Voice Dimmer with the My Leviton app adds advanced features such as preset lighting levels, fade rates, and bulb types and enables even more functionality to create lighting schedules and scenes such as “Movie Time” or “Dinner Time”.
Additionally, with Vacation Mode and Auto-Shutoff features – users can randomize their lighting for a lived-in look while away or set their Voice Dimmer to automatically turn of the lights after a preset amount of time.