Loading...

How many wireless devices can I connect to my home network?

The My Leviton App can support up to 99 Leviton Decora Smart Wi-Fi devices within a residence.  For customers looking to install a large number of devices it is recommended to consult the wireless network’s access point specifications to determine the maximum number of supported Wi-Fi devices.  In some cases, for example large installations, it may be necessary to upgrade to newer high performance wireless grade access points to ensure proper operation.