Loading...

Configuring the Dim Bar LED Behavior on a Decora Smart® Wi-Fi in-wall Dimmer

The LED indicators on the side of the dimmer can be programmed to be Always On, Always Off, or to timeout after a predefined period of time.

Tap the ⋮ in the device card and then tap Settings.

Devices
Devices

Select Device LEDs.

Devices

Select the Led Lightup Timeframe drop down and select the setting.  Once selected tap OK and then Save.

Devices
Devices
  • Always Off  = LED Bar is always off
  • 1 - 25 seconds = Time the LED bar will stay on after the light changes status
    • Default is 3 seconds
  • Always On  = LED Bar is always on