Loading...

Can I Integrate My Leviton With Google Nest Presence Detection

Nest Thermostat Presence Detection can be used to automatically turn My Leviton lights on or off.  The integration is accomplished in the Google Assistant app.

Nest
  • Both Home and Away Routines can use the Presence detection in the Next Thermostat to determine if you are home.
  • Either of these routines will allow you to add My Leviton lighting control when the household mode changes between home and away. 
  • Choose either the Home or Away routine
Nest
  • Presence can be detected based on voice command to a Google Alexa, mobile phone location and the sensor in Nest thermostats. Those settings can be changed in the Starters options.
  • To control the My Leviton lights, select the “Add action” 
Nest
  • All of the lights available via Google Assistant will be listed
  • Choose the My Leviton Light(s) you wish to control
  • Choose Next
Nest
  • Choose if you would like light(s) to turn on or off and if the device is a dimmer, set the dim level
  • Choose 'Add Action'
Nest
  • The newly created action(s) will be shown
  • Press Save
Nest