Loading...

Can I have more than one Residence?

Yes! My Leviton supports up to 20 residences for each account.

To add an additional Residence:

  • Select the Add Button (+) in the middle of the bottom navigation bar.
  • Now select Location.
Devices
Devices
  • Select the kind of location your are adding, Residence or Business.
  • Enter the location name in the space provided and then tap Next.
Devices
Devices
  • In the next step, you are prompted to enter the address for the residence.  The address information is used to set the correct time zone and calculate sunrise/sunset times for the Decora Smart devices.  You can select Use Current Location, Search by Address, or Skip for Now.  If you select to skip the location information you will not be able to create any automation schedules.  You can always add or change the location information at any time by modifying the Residence Settings from the menu.  

Setting Up the Location:
Select Use Current Location to use your mobile device's Location Service to determine the current location.

In response to Is this address correct?  verify the information is correct and select Yes.  If the displayed location is not correct, then select I'll enter it Manually to manually enter your location 

Devices
Devices
Devices
Devices

Once the address is confirmed you will be prompted to add devices to the location.